B-L462E-CELL1 Application Software
Hi,
I searching for the application example for the B-L462E-CELL1 Board.
In the Wiki it says:
The following hardware setup (B-L462E-CELL1) embeds more functionalities than other hardware setups. It also includes BSP for sensors and display, as well as a complete IoT application that displays information on the screen, reads humidity, pressure, temperature sensors, and uses cellular middleware to exchange with the network (Echo, Ping).
Where can I find an application which for example sends data to a cellular network?
The website offers two ZIP folder for the x-cube-cellular expansion:
- X-CUBE-CELLULAR
- XCC_FreeRTOS
The first one only has one Project called "Nx_TCP_Echo_Client", the second one has "Cellular", "Cellular_PPP", "CellularIoT".
However in the UM2426 User Manual, this Figure is shown:

Which states, that the "Cellular" Example is inside the X-CUBE-CELLULAR expansion... but it isnt. If you download it, only the "Nx_TCP_Echo_Client" is in there.
Do I have to merge the two folders? Can I install examples via the CubeIDE?
I just need an application example for the board and a manual on how to download the firmware to the board... The documentation is very unclear and not helpful at all...
Thanks for your help.
Best Regards