Backward compatibility
Hi, for our development we have selected "STM32F207ZG". The eval board which I see for MCU is "NUCLEO-F207ZG", which has pin-outs but not the required hardware interfaces on-board (usb-c fs, micro-sd, lcd, fsmc).
The dev board "32F469IDISCOVERY" has some on-board interfaces but based on M4.
Questions:
1. Can M4 program be directly reused for M3. Any changes in compilation, as M4 has DSP hardware?
2. Suggestions for dev board for above requirement.
3. Does FreeRTOS have support for M3, M4 and necessary interfaces
4. Can the interfaces be done without FreeRTOS libraries.
Request to look into above queries.