Battery powered B-U585I-IOT02A
I'm building a simple application that collects environmental data from sensors (pressure, temperature and humidity) using the B-U585I-IOT02A development board. Since I want to deploy the node directly on the field, I'm planning to power the board using several AA batteries through the VIN pin.
In order to estimate the battery life, I tried to measure the power consumption of the chip only using JP3, and of the entire board with a source meter in VIN.
Regarding the consumption of the chip alone, I get an average of 2 mA, a value that seems consistent with what is stated in the manual. While for the whole board, I get about 170 mA on average with a 5 V supply. Also, I notice that the ST-LINK debugger remains unnecessarily powered.
Why is the total consumption of the board so high? What can I do to reduce the consumption and have a longer battery life?
Thanks in advance.