Bootloader via USART1 on NUCLEO-WL55JC1 Nucleo-64 board (MB1389)
I'm trying program FLASH via serial bootloader using STM32WL55 USART1
The an2606 indicates that
- USART-RX is PA10 pin, connected to CN7-32
- USART-TX is PA9 pin, connected to CN10-19
I connected the BOOT0 pin to 3.3V
- If after reset I send 0x7f to LPUART via ST-LINK VCOMM I get ACK (0x79) back
- But if after reset I send 0x7F to PA10 using external FTDI232 adapter I'm not getting anything back. If I check level of PA9 it shows 200mV (the PA10 is 3.3V) with FTDI connected and 0V with FTDI disconnected
- The loopback test on FTDI is working fine, so I don't suspect FTDI malfunctioning
I suspect my board is not properly configured, but could not see anything that would affect PA9 and PA10 configuration.
Can it be an error in a board documentation, I already spotted one error in table 18, it shows both CN10-35 and CN1-37 connected to PB6, which is probably wrong, one of them must be PB7.