Brand new STM32F769I-Disco board shows only black screen
Hi Folks,
Just received the STM32F769I-Disco Discovery board. I made sure the that the CN3 jumper was on the STLK position. When I plugged in the USB connector nothing happens on the screen it stays black.
I found a previous post dated 2023-07-06 10:07 AM "Brand new STM32F769I-DISCO board showing black screen"
This user seems to have had my exact problem. Not sure why these boards are being shipped blank.
I followed the instructions that Aime (ST employee) suggested. I downloaded the compiled demo "STM32769I-DISCO_DEMO_V1.0.0_FULL.hex" and using the STM32CubeProgrammer I think I loaded it onto the board. I say "I think" because when I reset the board the backlight turns on and "life.augmented" shows up at the bottom of the screen but that's it, nothing else.
The only thing I can think of that I did wrong is maybe I didn't load the file at the proper address? What is the correct address? Is there something else I can try?
And my board had the same test sticker as the Wol (the other user with the same problem) on the board has T1-T4 all ticked, but no tick on the QA box.
Thanks,
Richard