Skip to main content
Visitor II
August 17, 2020
Solved

[BUG] ST-Link firmware verification - No ST-LINK detected message since 1.4.x update.

  • August 17, 2020
  • 13 replies
  • 17990 views

On Windows 10, I just updated (again) to the 1.4.2 version, hoping to solve this issue, yet nothing changed.

Already tried a clean install (again) and re-installed the latest STM32CubeProgrammer: nothing changed.

Will ST handle this sooner or later please? Or at least give some help in diagnosing the problem? Thanks

    This topic has been closed for replies.
    Best answer by LaurentL

    Yes of course, it will be included for next releases.

    Edit after it was marked as best answer :

    The libusb dll v1.0.23 is now installed with STM32cubeIde v1.5.0 installer.

    So, no need to patch it, just install (not update) STM32CubeIde v1.5.0.

    Rgds,

    Laurent

    13 replies

    October 1, 2020
    Visitor II
    December 16, 2020

    I have had the same problem, and following the installation instructions of the dll file, everything works fine now.

    Thanks.

    ST Employee
    December 17, 2020

    Hi,

    You can install (not update) STM32CubeIde v1.5.0, the new libusb dll is installed now.

    Rgds,

    Laurent

    Visitor II
    August 5, 2023

    Hi,

    I have installed latest version of STM32CubeIDE which is 1.13.1. I am facing the same problem of ST-Link not detected. I tried solving the issue following your guides but it's not being resolved. If you could please guide me how can I resolve this issue. I would be really grateful. 

    Explorer II
    January 22, 2022

    So is there any fix for this yet?

    STM32CubeProgrammer 2.9.0 can't even detect the L031K6 nucleo st link.

    STM32CubeIDE 1.8.0 does see it but won't use it.

    Fortunately I can update it to mass storage mode, that works, but debugging would be nice.