Can an ST Link V3MINI be changed to a V3MODS?
I'm designing some service hardware for a product which needs to program an STM32L4 chip, write a few values to an I2C EEPROM and send a few commands over a UART to run diagnostic functions.
The ST Link V3MODS seems an ideal tool for this as it has all the interfaces. Trouble is, nowhere has stock and most are saying 2023 before more is due. I've got a few V3MINIs, do these support the same functionality out of the box, or can they have the V3MODS firmware programmed on to them? Easy enough to remove the few components on the bottom I don't need, so is this viable?
Other option would be the V3SET but this would need some cumbersome cabling making, while the V3MODS can sit on a PCB with a few other bits I need for the diagnostics.