Skip to main content
Graduate
March 26, 2025
Question

Can I Use ST-LINK/V2-1 from Nucleo-F446RE to Program an External STM32 MCU?

  • March 26, 2025
  • 2 replies
  • 663 views

I have an STM32 Nucleo-F446RE, which comes with an integrated ST-LINK/V2-1 debugger. I would like to use this ST-LINK to program an external STM32 MCU that does not have a development board.

  • I checked the Nucleo schematics, and I see that ST-LINK/V2-1 can be used for external programming.

  • I know that I need to connect SWDIO, SWCLK, GND, and  VDD to the external MCU.

  • I removed the two jumpers from CN2 to disconnect ST-LINK from the onboard STM32F446RE.

Before proceeding, I want to confirm if this setup is correct, if I need additional components like resistors or capacitors, or if I should buy a dedicated ST-LINK V2 instead.

I appreciate any guidance to help me solve this problem.

Thank you in advance.


    This topic has been closed for replies.

    2 replies

    Technical Moderator
    March 26, 2025

    Salam @MedSid and welcome to the ST Community.

    Your setup should be working just fine. You can use the ST-LINK/V2-1 from Nucleo-F446RE to Program an External STM32 MCU. More details are available on the answer of this post and UM1724.

    Best Regards.

    STTwo-32

    Super User
    March 26, 2025