Can not flash stm32f407vet6 with st-link v2 programmer.
After unsuccessful firmware, via cubeide (debugger was not selected), the microcontroller is not flashed via st-link v2 (swd). Tried in 1) cubeide, 2) cube programmer, 3) st-link utility.
1 File to start the GDB server
2 The firmware of the programmer was updated with a signal to BOOT0, but he does not want to program the chip and does not see
3 In connection mode, when reset, the error: "... select a lower frequency SWD mode ..."
What can be done and what is happening? Please help me figure it out.