Skip to main content
Visitor II
July 25, 2019
Solved

Can not set "nBOOT_SEL" bit in STM32L011F4 MCU.

  • July 25, 2019
  • 2 replies
  • 1990 views

Hello, everybody.

I am developing one small application, using STM32L011F4 MCU. As I realised from datasheet, there are two ways to boot from flash memory:

1)Connect PB9-BOOT0 pin to ground;

2)Set nBOOT_SEL bit and use nBOOT0 bit instead of BOOT0 pin.

Also, datasheet says that nBOOT_SEL bit available only for Category 1 devices.

0690X000009Z68IQAS.jpg

Again, according to datasheet, STM32L011F4 is category 1 device:

0690X000009Z68cQAC.jpg

The problem is that I can not program nBOOT_SEL bit using ST-LINK UTILITY, it is shown in gray color and I can not check/uncheck it.

0690X000009Z68rQAC.jpg

What could be the problem?

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    Try the STM32 Cube Programmer, it is the software they have migrated too.

    2 replies

    Graduate II
    July 25, 2019

    Try the STM32 Cube Programmer, it is the software they have migrated too.

    MPiskAuthor
    Visitor II
    July 25, 2019

    STM32 Cube Programmer works fine, thank you very much.