Skip to main content
Visitor II
June 2, 2019
Question

Can st-link be configured in STN32CubeIDE?

  • June 2, 2019
  • 3 replies
  • 1044 views

My target is STM32F103C8T6. My project works when I generate a .bin file and upload it using the stand-alone st-link utility configured as "connect under reset". I cannot upload directly from the IDE, I get the errors:

-----------------------------------------

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

--------------------------------------------------

Any tutorials on how to configure st-link in STM32CubeIDE?

Thank you!

    This topic has been closed for replies.

    3 replies

    Visitor II
    June 8, 2019

    I am also looking for an answer on this topic. Were you able to successfully perform Debug using ST-LINK GDB SERVER?

    I'm also getting the above error. Please let me know you are able to program the target through STM32CUBEIDE?

    Visitor II
    June 10, 2019

    I never found a way so have been using an external utility.

    Visitor II
    June 24, 2019

    I have a sample problem.

    I'm using NUCLEO-F103RB with STM32CubeIDE V1.0.1

    STMicroelectronics ST-LINK GDB server. Version 5.2.3

    Copyright (c) 2019, STMicroelectronics. All rights reserved.

    Starting server with the following options:

        Persistent Mode      : Disabled

        Logging Level       : 1

        Listen Port Number     : 61234

        Status Refresh Delay    : 15s

        Verbose Mode        : Disabled

        SWD Debug         : Enabled

    Target no device found

    Error in initializing ST-LINK device.

    Reason: No device found on target.