Skip to main content
Graduate II
June 19, 2023
Question

Can X-NUCLEO-LPM01A be used for boards other than STM32?

  • June 19, 2023
  • 1 reply
  • 896 views

Does the X-NUCLEO-LPM01A allow to measure power consumption of boards like Pi Pico, Arduino Nano Connect RP2040? Or only Nucleo boards?

I have nucleo board to which i have connected GPS module, IMU, LCD display. Will the Power Shield measure power consumption of all those components or only the MCU which is on the Nucleo board?

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 19, 2023

    Hello @DPiór.1,

    yes, the X-NUCLEO-LPM01A can measure power consumption of all devices with Arduino Uno or Nano headers/pins using the integrated headers, or basically any target using the basic (white) connector.

    Concerning the consumption of other peripherals it depends on your configuration and connection of power pins - both variants are possible (assuming you are in the min-max current range of the expansion board).

    I recommend you to follow the user manual for the expansion board: https://www.st.com/resource/en/user_manual/um2243-stm32-nucleo-expansion-board-for-power-consumption-measurement-stmicroelectronics.pdf

    Regards,

    Jaroslav