Cannot connect the ST-Link V2 to my custom PCB "Error: No STM32 target found"
Hello,
I have been stuck trying to connect my ST-Link V2 to my custom PCB. I am confident that each of the connections made on the schematic are correct and that the solder joints are ok. I have tested everything with a multimeter. I have tried updating firmware, updating STM32CubeProgrammer, erasing board memory, flashing a program via USB that is configured to communicate via SWD, changing mode from normal to under reset, changing reset mode from hardware to software, and tried connecting with BOOT0 pulled high and low. I am using an STM32F446RCT6 with PB2 pulled low. Sorry if I am missing any information that may be useful. Any guidance is appreciated.
Schematic is above. It is very rough as this is just a quick and dirty test board for the IMU attached. The pin numbers don't even match the datasheet for the MCU but the position of each pin does correspond to the correct pin. Also, the 1uF cap has been replaced with a 100nF cap on the reset line.