Cannot reflash my STM32G030F
I've designed a board that uses an STM32G030F6 processor.
Now I've updated the software and... (one feature wasn't implemented yet) I cannot connect to the target CPU to flash tne new firmware into the board.
Then you'd think I've programmed the SWD pins to something else that AF1: SWD, but as far as I know: i haven't.
That said, then I should be able to use "connect under reset" and again... that doesn't work. (It should work if I manually hit the reset button, right? )
Both programmers I've tried today program my STM32F072R development board just fine without any trouble.
Any suggestions?
I thought: Maybe there is a way out with the bootloader, but alas, I've not hooked up the "boot0" pin to the programming connector as I usually do... The reason being that by default the 'G030 doesn't have a boot0 pin: that isn't enabled in the default flash config and the pin conflicts with SWD.
I'm a Linux user, don't have access to MS Windows. I use "stlink" software by Texane .