Clock mismatch in template code for NUCLEO-L412RB-P?
Hi there, we are getting started with a NUCLEO-L412RB-P evaluation board, which has a stm32L412RBT6PU processor on it.
According to Section 9.7.1 of the user's guide (UM2206), the default clock is the LSE oscillator, which is "OSC 32khz clock supply."
However,in the cubeL4 code, \Projects\NUCLEO-L412RB-P\Templates_LL\SRc\main.c file, they have the code below, which suggests 8MHz.
Is this a mismatch? Out of the box, do I need to change either my nucleo board clock, or the 80000000 below, in order to get it to work properly? Or (probably more likely) is there something I don't understand, and what is that?
Thanks!
/* Set systick to 1ms in using frequency set to 80MHz */
/* This frequency can be calculated through LL RCC macro */
/* ex: __LL_RCC_CALC_PLLCLK_FREQ(__LL_RCC_CALC_MSI_FREQ(LL_RCC_MSIRANGESEL_RUN, LL_RCC_MSIRANGE_6),
LL_RCC_PLLM_DIV_1, 40, LL_RCC_PLLR_DIV_2)*/
LL_Init1msTick(80000000);
/* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */
LL_SetSystemCoreClock(80000000);