Commands LORA: P-NUCLEO-LRWAN2
Hi,
I recently bought a P-NUCLEO-LRWAN-2, and I would like to communicate through LORA from the gateway to the end-node and vice-versa, but some information is lacking.
In the Getting started with the P-NUCLEO-LRWAN2 and P-NUCLEO-LRWAN3 starter packs DOC there is no inofrmation on how to send and receive data, for example, with the command LORA_send() I saw on a website, and the file USI WM-SG-SM-42 AT Command cannot be found, and the link given at [1] doesn't lead me anywhere.
Could you pls give me this information on how to receive and send data, or where can I see that Info. I don't need to use for now a dashboard, it would be enough to just put something on a terminal on one of the modules, and just see if the info was received on the other terminal, for example.
I also know that the end-node has some sensores, how can I access them?
Thanks for your attention.