Compatibility of STLINK-V3MODS SWD Pins with 3.3V MCU Logic Levels
Hello ST Community,
I have a question regarding the compatibility of the STLINK-V3MODS SWD pins with my MCU's SWD pins, which operate at 3.3V. Do I need to use logic level shifters between them, or are the STLINK-V3MODS SWD data signals fully compatible with 3.3V logic levels? Additionally, can I connect them without using logic shifters, and if so, would that be safe for stable operation?
Thank you for your assistance!