Skip to main content
Visitor II
June 8, 2017
Question

Concerning ST-Link on Nucleo Board

  • June 8, 2017
  • 1 reply
  • 1560 views
Posted on June 08, 2017 at 17:33

hi,  fellows!

I have some questions about ST-Link, especially those on Nucleo boards.

First, I often use the on board st-link link to debug/program some other custom boards, it works fine.

But someday, I'd noticed that the debugger's AIN_1(target VCC) is never  really connected to the MCU VCC

of the application board, for R9 is not lying there. See below:

0690X00000607H3QAI.png

From the UM1075 User manual of ST-Link, it says:

The power supply from the application board is connected to the ST-LINK/V2 debugging and programming board to ensure signal compatibility between both boards.

So is this really unnecessary? (For me, the debugger/programmer works fine so far.)

Or is this risky for some reason?

I really need to know about this!

For we are making a project with the whole nucleo board as a part,

 with st-link on it.

And I've already removed R23 for saving power.

See below:

0690X00000602TEQAY.bmp

Thanks for reading the post!

Zt

#debugger #st-link #programmer #nucleo
    This topic has been closed for replies.

    1 reply

    Graduate II
    June 8, 2017
    Posted on June 08, 2017 at 20:00

    The stand-alone ST-LINK has buffers so that the debugger and the target board can run at different voltages. The NUCLEO/DISCO boards don't have these buffers, and just use/assume the use of 3.0V or 3.3V signalling.

    Most of the pins are 5V tolerant, and the VIL/VIH vs VOL/VOH provide a lot of leeway.

    The idea would be to avoid back-feeding current into a processor via the GPIO pins and skewing the current measurements.

    If the target STM32 were running at 1.25V I'd probably want the buffers

    Zt LiuAuthor
    Visitor II
    June 9, 2017
    Posted on June 09, 2017 at 01:14

    Thanks Clive, as always!

    So since my target MCU is running at 3.0/3.3V, there is a lot of leeway.

    Guess I can sleep well with the target VCC pin left open! 

    :)