Connecting 8ohm speaker to stm32H743 EVAL Board.
Hi ST,
I am using a stm32h743I EVAL Board and trying to connect the 8ohm speaker on CN19. I am using SAI_AudioPlay example from the STM32Cube_FW_H7_V1.11.0 package. I have followed the readme file and got the headphones working fine; to make the speaker working, I have changed the lines below in the main file.
codec_init.InputDevice = WM8994_IN_NONE.
codec_init.OutputDevice = AUDIO_OUT_DEVICE_SPEAKER.
codec_init.Volume = VOLUME_IN_CONVERT (60).
But can't heard any sound out of my speaker and after analyzing the init function inside the wm8994.c file, I have done some modifications and the I can be able to hear the sound through speaker, but the sound is very low.
Can anyone suggest me, is there any possibility to increase the volume on the speaker, I have gone through almost all the registers and tried increasing the sound of the speaker but failed. Any help really appreciated.
Thanks,
Murali Chikkanna