Connecting G0 Nucleo board to Linux
I've been running into issues with my G0 Nucleo board in that I can't seem to get it to connect properly to my Linux machine via STLink. I've gone through and added the requisite rules, but even so if I list USB devices, the board is conspicuously absent and the status lights on the STLink module continue to blink red. How can I determine whether this is an issue with my software or an issue with the board itself? For either situation, what remedies do I have at my disposal?
PC runs Ubuntu 20.04, if that's relevant.