Skip to main content
Visitor II
December 22, 2020
Question

Cube ide 1.4 doesn't recognize nucleo 32 board on linux.

  • December 22, 2020
  • 1 reply
  • 749 views

I have an STM32 Nucleo 32 (F303K8) and was able to use it before. But 1.4 doesn't seem to recognize the boards. I even connected STLink-v2 device and even that did not get identified.

    This topic has been closed for replies.

    1 reply

    Graduate II
    December 22, 2020

    Starting STM32CubeIDE 1.4.0 ST-Link server driver is required. Have you installed it ?

    Takes care if updating (Thnaks Help>Check for Update) from some release to 1.4.x such drivers are not managed. Only fresh install starting from installer is supporting such.

    By the way consider 1.5.1 latest release if possible doing fresh install.