Cube Programmer crashing dual core microcontroller when using STLink-V3SET
Hey folks,
I'm trying to load firmware onto an STM32H755BI Microcontroller (Dual M4-M7 core). When loading the M7 core with new firmware, I have no issues. However, when I load the M4 core the microcontroller crashes badly. I've tried loading via CubeProgrammer and through a gdb-multiarch instance attached to stlink-gdbserver, but both have the same result: both the M4 and M7 cores crash, and cannot be reset through `run`, `mon reset`, or `mon hardware_reset` commands.
Here is the output when I try loading with GDB:
```
(gdb) load
Loading section .isr_vector, size 0x298 lma 0x8100000
Loading section .text, size 0x7ce0 lma 0x8100298
Loading section .rodata, size 0x9c lma 0x8107f78
Loading section .ARM, size 0x8 lma 0x8108014
Loading section .init_array, size 0x4 lma 0x810801c
Loading section .fini_array, size 0x4 lma 0x8108020
Loading section .data, size 0x20 lma 0x8108024
Loading section .RxDecripSection, size 0x60 lma 0x8108044
Loading section .TxDecripSection, size 0x60 lma 0x81080a4
Start address 0x810170c, load size 33028
Transfer rate: 26 KB/sec, 1738 bytes/write.
(gdb) c
Continuing.
Program received signal SIGTRAP, Trace/breakpoint trap.
0xa05f0000 in ?? ()
```
With CubeProgrammer, the processor shows that it is in the "Halt" state after completing a load. If I try to start running, a popup window says "Error : Unable to run application".
Note that in both instances, the firmware load succeeds. However, I am unable to connect to the microcontroller unless I power cycle it.
I've also tried loading firmware using the Segger J-Link, and it is able to load the M4 core without any notable issues.
Any ideas as to what the issue is here, or if it is fixable on my end? As far as I can tell this is a STLink-V3 firmware problem.