Custom board works normally when attached to STlink but does not boot in standalone.
Hello!
I guess most of the problem is described in the title. I made a board using a STM32F767 chip. It works well when attached to STLink, can be debugged and programmed, communicates well by SPI and so on. But once detached from STLink, it doesn't boot at power up.
This chip has only a Boot0 pin, which is high. I also verified that NRST is high, The ST link connection uses a 10 pin connector from a mini STLink V3.
Sometimes the board boots by simply attaching STLink V3 mini. I tried to touch any of the pins of the STLink connector, start with pins at 0 or 1 at startup, no way to make it boot.
Does anybody know what could be wrong?
Any hint welcome.
Thanks!