Custom STM32F413 Will Not Connect With STLinkv2
Hello! I am developing a custom stm32f413rgt6 board to interface with a thermal camera. I am having some difficulty getting my first upload going on STM32CubeIDE and would really appreciate some help. I believe my hardware schematic is sound, and the issue is something with settings. Nonetheless, I will attach everything. Here is my error from CubeIDE:

My settings:


Im using an STLinkv2 from Digikey and have connected the VCC, SWDIO, SWCLK, and GND. Since the system is getting 3V, I also tried modifying the hardware to boost it up to 3.3V which succeeded hardware-wise but did not resolve my problem.
I have SYS configured on CubeIDE as well:

I attempted also connecting it to CubeProgrammer but am unable to establish communication with the board from the STLink. I kept getting:

Per settings:

I also tried uploading with RST pin pulled low per the setting above to no luck on both programmer attempts. I'd very much appreciate any and all assistance!
Thank you,
Justin