Daignose Nucleo-h563zi and how to repair it
I was using Nucleo-h563zi board in which my application was to run it using external power source so for that i shifted the jumper to E5V to power the board usign external 5V. I was using AMS1117 voltage regulator to convert it to 5V from 12V but accidentaly due to failure or it 12V was given to E5V pin after the LD4 and LD6 led is red and the LD5 is not turning on as usual when the jumper is shifted to STLK for programming.
After this when i try to program by changing the jumper to STLK it is detected but while uploading it is showing "No stlink device found"
i found that the 5V,3.3V is shot circuited. what is the possible reason and how to repair it.
Can you please suggest some way to repair it.