Debug STM32F0 with SWD (STLINK - V3) - ANSWERED
Hello,
I want to program (first time) an STM32F042K6 with STLINK-V3SET using SWD.
When I try to "connect" with STM32CubeProgrammer, I get these informations : "Error : No STM32 target found!". Here is a screen :

The connections are :

I tried to run the µC forcing PB8(BOOT0) low and high, but I got the same problem.
I have some ideas but I didn't find anything in the docs :
1) I'm using STLINK-V3SET with MB1440B, it is an extension board provided by ST. Is there any jumper we need to add or remove (according to the docs, I would say no but...)
2) Maybe STM32CubeProgrammer configuration is wrong ?
3) It is the first time I program this chip, maybe I need to use the bootloader ?
Thank you,
Best regards,
Valentin