Debugging external MCUs with STM32F746-DISCO and STM32769-DISCO
Are STM32F746-DISCO and STM32769-DISCO ST-Link not supposed to be used to debug external STM32s? The T_NRST (the pin that controls the NRST pin of the target MCU) is not given out in the SWD connector, it can only be indirectly reached through the on board MCU's NRST pin. Moreover, I could not have seen any headers to cancel out the other connections between ST-Link and the on Board MCU.
Can these two boards be used to debug external MCUs and leave the on board MCU unattended while doing so?
Regards
Den
#st-link #stm32f746-disco #stm32769-disco