Skip to main content
Visitor II
May 31, 2021
Question

Debugging probe StLink V3 MINI vs MODS ? Why MODS does not work via CN5 connector?

  • May 31, 2021
  • 2 replies
  • 1208 views

Hello,

I bought the StLink V3. The MODS version. The idea was to have good, handy and slim debugging probe. Well isolated as housed in thermally shrinking tube.

I equip all my Stm32 pcbs with the miniature debug connector comprised of: Gnd, SwCk, SwDio, Swo so such a slim probe would be very appreciated.

Fist I connected to the connector CN5 and... got message that "Error... No device found on target". Hmmmm. why?

After an investigation I discovered the differences between version MODS and MINI. Photo shows that MINI has more components assembled.

So I moved to CN2 edge connector (pins 4,8,13) and now my probe works well :-).

So could you please clearly mention in the datasheet (as engineer for engineer) that MODS differs from MINI and how? I agree that you formally inform "...This function is available on CN2 (STLINK-V3MODS) and CN5 (STLINK-V3MINI)...." but such a warning would be useful, I guess.

Could you reveal what components should I add to my MODS to get signals on CN5 connector? I guess they are buffers giving more security for delicate CN2 inputs of probe board? The next probe I will buy will be the MINI (and I will remove the CN5 smd connector) but I would be happy to reinforce my current MODS too.

All the best

Robert

    This topic has been closed for replies.

    2 replies

    Super User
    June 1, 2021

    Would be nice if they just provided the schematic like they do for so many other boards. No idea why this one is an exception.

    Explorer II
    June 1, 2021

    As you can guess from fig. 8 in UM2502 there are 8 resistors missing on the bottom side. For each of these resistors, one pad is connected directly to a pad on CN5, the other one directly to CN2. The missing resistors are due to the fact that STLINK-V3MODS is intended to be soldered on a PCB, they would be in the way. Most certainly any value in the range 100 ... 1k Ohms will do. The two missing 5-pin devices on the top are connected to T_NRST and T_JCLK, respectively, but they're apparently not necessary as you got it working via CN2.