Decoupling capacitor placement
Hi,
I am currently optimizing some designs and started thinking about decoupling capacitors. As far as I know, it is a rule of thumb to place "one 100 nF capacitor per V+ pin".
In the attached document, ST recommends exactly this. Let´s look at the document: n x 100 nF + 1 x 4,7 uF. I interpret this in the following way: For each VDD pin, I have to place one 100 nF capacitor (as close as possible to the pin) and, overall, I need an additional 4,7 uF capacitor.
Now two questions arise:
-If you look at pins 33, 34 and 35, do I really need three single 100 nF capacitors? Couldn´t I just place one 300 nF in the middle? Or maybe one 100 nF would also suffice?
-Where do I place the 4,7 uF capacitor? The pins are quite far apart. Do I just place it "somewhere"?
I think I understand the theory that the capacitors serve as an energy buffer when the uC has transient changes in current draw and that they filter out high frequency spikes on the traces.
I have a two layer PCB and I am looking for a practical answer for this particular case.
Kind regards
René