Skip to main content
Visitor II
January 11, 2021
Solved

Different HW-Versions of ST-Link/V2

  • January 11, 2021
  • 3 replies
  • 1749 views

Hello Forum,

recently I bought me a new ST-Link/V2 to program and debug a STM32L4. I tried to connect the programmer with the MCU, but it didn't work. Now I tried it with a different programmer and I could establish a connection to the STM32L4. After that I tried to connect the new programmer with a STM32G0 and this also works.

Version of new programmer: ST-Link/V2 A2020 03

Version of old programmer: ST-Link/V2 B2017 15

Both programmers have the same Firmware Version.

Could anyone please tell me where the error is?

Kind regards

Eric

    This topic has been closed for replies.
    Best answer by Eric_Z

    Hello,

    thank you for your answers. But a few weeks ago I talked to an ST employee and showed him the schematic of the STML4. I forgot the 100 nF capacitor at Reset...

    Kind regards

    Eric

    3 replies

    Graduate II
    February 10, 2021

    Carefully and double check all connections, USB cables and USB ports, I do not think there is a real functional difference in both versions.

    Graduate II
    February 10, 2021

    Are these authentic or clones?

    Watch that you're powering pins 1 or 2 with VTarget so as to power the buffers.

    Super User
    February 11, 2021

    "Are these authentic or clones?"

    +1

    If you've got cheap clones like this from ebay or the like:

    0693W000007EoJJQA0.pngbeware that there are at least two different pinouts on otherwise identical-looking products!

    EDIT

    Here you go:

    0693W000007EoKCQA0.pngClick the image to enlarge - Look carefully at the two pinouts!

    Eric_ZAuthorAnswer
    Visitor II
    February 11, 2021

    Hello,

    thank you for your answers. But a few weeks ago I talked to an ST employee and showed him the schematic of the STML4. I forgot the 100 nF capacitor at Reset...

    Kind regards

    Eric

    Super User
    February 11, 2021

    Thanks for the update - it would have been helpful if you had said that earlier!

    So that the forum shows the issue as solved, please 'Select as Best' on your answer:

    0693W000007EqSXQA0.pngThen the 'Answered' flag will be shown in the forum listings:

    0693W000007EqUJQA0.png