Different patten when same output frequency at differernt pin. (NUCLEO-H563I)
I tried to set the SPI CLK to 20MHz at VDD=1.8V, but there was no output signal at PB13. When I change to 5 MHz it returns to normal, but the waveform seems to have been filtered by the low-pass filter. Finally, I set it to 2.5MHz to make it work stable. However, the patterns between PG11(C2) and PB13(C1) at the same frequency are different.

I want to confirm. Is that issue because the layout routing distance different between these two pins on the board? If I directly probe the IC pin, the pattern will be the same, right?