DMX decoder using STM32 H7
Hello everyone,
I am trying to receiver a DMX frame using STM32 UART interrupts. I'm trying to receive the data byte-by-byte using a state machine logic. The problem I am facing here is that none of the debug LED code to toggles the LEDs when the program hits a certain point. I just need to decode the DMX code byte-by-byte to process the frame and detect the 'break' bit by the Error callback. Is the logic correct or do I need to find another solution?
It would be massively helpful if anyone could help me with this.
Here's the code (initialization code excluded and everything initialized as per DMX standard):
#define MAX_BYTES 10
volatile uint8_t current_bytes[MAX_BYTES];
volatile int byte_index = 0;
typedef enum {
WAIT_FOR_BREAK_BYTE,
BREAK_CONDITION,
WAIT_FOR_FIRST_BYTE,
READ_DATA
} USARTStates;
volatile USARTStates USART_state = WAIT_FOR_BREAK_BYTE; // Initialize the state to the initial state of the machine
volatile int IsBreak = 0; // Flag to indicate if a break has been detected
volatile uint8_t DMX_Buffer[513]; // The DMX data buffer; Plus 1 for the start byte.
volatile int DMX_Counter = 0; // Keeps track of the current byte number in the DMX sequence (0-512).
volatile int DMX_address = 1; // The address of the channel you want to listen to
volatile int DMX_index = 0; // Index for storing received DMX bytes in DMX_Buffer
volatile int DMX_channels = 512; // Maximum channels
volatile int valid_DMX = 0; // Flag to indicate if received DMX is valid. You can use this in other parts of your application.
volatile uint8_t DMX_val[10];
void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
{
uint32_t error = HAL_UART_GetError(huart);
if (error & HAL_UART_ERROR_FE)
{
IsBreak = 1;
DMX_Counter = 0; // Reset DMX counter
byte_index = 0; // Reset byte index for current_bytes
}
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
switch (USART_state)
{
case WAIT_FOR_BREAK_BYTE:
// Managed by ErrorCallback for detecting break.
break;
case BREAK_CONDITION:
if (current_bytes[byte_index] == 0) // Check for the start code
{
USART_state = WAIT_FOR_FIRST_BYTE;
DMX_Counter = 1;
byte_index = 0; // Reset byte index for next bytes
}
else
{
USART_state = WAIT_FOR_BREAK_BYTE; // Not the start code, wait for next frame
}
break;
case WAIT_FOR_FIRST_BYTE:
byte_index++; // Increment index to store next byte
DMX_Counter++;
if (DMX_Counter == DMX_address)
{
DMX_index = 0; // Reset index for DMX_val
USART_state = READ_DATA;
}
break;
case READ_DATA:
DMX_val[DMX_index++] = current_bytes[byte_index];
DMX_Counter++;
byte_index++; // Increment index to store next byte
if (DMX_index == DMX_channels)
{
USART_state = WAIT_FOR_BREAK_BYTE; // All channels read, wait for next frame
}
break;
}
// Make sure not to overrun the array
if (DMX_Counter <= 512 && byte_index < MAX_BYTES)
{
HAL_UART_Receive_IT(&huart4, ¤t_bytes[byte_index], 1);
}
}