Question
Does ST-LINK Utility support multiple devices on JTAG chain?
Posted on January 07, 2015 at 23:54
I have a system with multiple STM32F407 MCUs. The JTAG signals are daisy-chained together into one long chain.
Can I use the ST-LINK Utility to flash firmware into a specific device on the JTAG chain? I looked through the user manual but did not find any settings to select which device on the JTAG chain to program. I'm able to do this with a different hardware pod (J-Link from Segger), but I was hoping to use the ST-LINK/V2 pod since it costs 90% less. Thanks for your time! Tim #st-link #jtag