Skip to main content
Visitor II
February 6, 2023
Question

Does TCPP01-M12 Source Pin (pin 4) really have a 5.5V Absolute Max voltage limit?

  • February 6, 2023
  • 1 reply
  • 773 views

Table 3 of DS12900 - Rev 6 shows a max voltage of 5.5V, which doesn't make sense, unless I'm missing something very important.

Is this just a typo? Seems like it should be on the same line as the GATE pin or IN_GD.

Thanks

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    February 9, 2023

    Hello @bdieh.1​ and welcome to the Community :)

    Thanks for pointing out this issue. 

    I confirm, it is a typo: SOURCE PIN ARM is 24V. As you write it is the same value as IN_GD.

    An internal ticket ID 145127 is submitted in order to update the Datasheet.

    (PS: ID 145127, this is an internal tracking number for reference and is not accessible or usable by customers).

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen