Skip to main content
Visitor II
July 5, 2022
Solved

Does the STLINK-V3SET need back bias protection when unpowered?

  • July 5, 2022
  • 1 reply
  • 750 views

Specifically, when T_VCC is not supplied, what state are the pins in for the STLINK-V3SET? We are using the SWDIO, SWCLK, and JTAG pins on the STDC14 connector CN1.

    This topic has been closed for replies.
    Best answer by LauraCx

    As the STLINK-V3SET is designed around the STM32F723 microcontroller, it will follow the STM32F723's embedded internal pull-ups and pull-downs on the JTAG input pins:

    • NJTRST: Internal pull-up

    • JTDI: Internal pull-up

    • JTMS/SWDIO: Internal pull-up

    • TCK/SWCLK: Internal pull-down

    1 reply

    LauraCxAnswer
    ST Employee
    September 15, 2022

    As the STLINK-V3SET is designed around the STM32F723 microcontroller, it will follow the STM32F723's embedded internal pull-ups and pull-downs on the JTAG input pins:

    • NJTRST: Internal pull-up

    • JTDI: Internal pull-up

    • JTMS/SWDIO: Internal pull-up

    • TCK/SWCLK: Internal pull-down