Skip to main content
Visitor II
November 4, 2025
Question

EC200U connection lost after receiving 2 min of image raw data

  • November 4, 2025
  • 0 replies
  • 113 views

Hi all, 

I am transmitting and receiving the image data using AT commands via UART in stmf767vi board. 

My transmission is sending successfully like sending chunk by chunk. I am able to see the count also. But the problem is while receiving side, I am able to receive the chunk for 2 min only. not all the image. If tx image size is 80k, I am able to see upto 35k only. after that my mqtt is stopping receiving the image data. I don't know where it is causing whether it is keep-alive timeout or something else. Even when I am receiving the small size data, it is receiving 6 times the full image like upto 2 min. after that it is stopping. what is the issue ? someone please help...

 

while(1)

{

 

receive_data_test((char *)&response[0], RX_BUFFER_SIZE, 60000);

}

 

 

eState_t receive_data_test(unsigned char *out_buf, uint16_t buf_size, uint32_t timeout_ms)

{

uint32_t last_ping_time = HAL_GetTick();

 

uint8_t rx_byte;

rcvdCount = 0;

notRcvdCount = 0;

while (1)

{

if (HAL_UART_Receive(&huart3, &rx_byte, 1, 10) == HAL_OK)

{

rcvdCount++;

notRcvdCount = 0;

}

else

{

notRcvdCount++;

if(notRcvdCount > 1000)

{

notRcvdCount = 0;

}

}

// one minute checking for keep-alive timeout

if((HAL_GetTick() - last_ping_time) > 60000)

{

// publish the command.

snprintf(cmd, sizeof(cmd), "AT+QMTPUBEX=0,0,0,0,\"keepalive/topic\",4\r\n");

send_at_command(cmd);

 

// Step 2: Waiting for '>' prompt

if (!receive_response_wait_for(">", response, RX_BUFFER_SIZE, 5000))

{

print("No '>' prompt received for QMTPUB\r\n");

errorStepNumber = 14;

return;

}

 

HAL_Delay(100);

send_at_command("ping\r\n"); // sending the payload

 

// Step 4: Wait for broker ack

if (!receive_response_wait_for("+QMTPUB: 0,0,0", response, RX_BUFFER_SIZE, 5000))

{

print("Keepalive publish failed\r\n");

errorStepNumber = 15;

return;

}

print("Keepalive sent successfully\r\n");

HAL_Delay(100);

 

last_ping_time = HAL_GetTick();

}

}

return state;

}

just checking the data reception is happening or not.

before the receive_test_data functions, I am sending the AT commands successfully.

send_at_command("AT\r\n");

send_at_command("AT+CSQ\r\n");

send_at_command("AT+CPIN?\r\n");

send_at_command("AT+CREG?\r\n");

send_at_command("AT+CGATT?\r\n");

send_at_command("AT+QIDEACT=1\r\n");

snprintf(cmd, sizeof(cmd), "AT+QICSGP=1,1,\"%s\",\"\",\"\",1\r\n", apn);

send_at_command("AT+QIACT=1\r\n");

send_at_command("AT+QIACT?\r\n");

snprintf(cmd, sizeof(cmd), "AT+QMTOPEN=0,\"test.mosquitto.org\",1883\r\n");

snprintf(cmd, sizeof(cmd), "AT+QMTCONN=0,\"clientid835\",\"\",\"\",0\r\n");

send_at_command("AT+QMTCONN?\r\n");

snprintf(cmd, sizeof(cmd), "AT+QMTSUB=0,1,\"image/data\",2\r\n");

 

    This topic has been closed for replies.