EDT Graphich Display with STM32F7 MCU
Hi guys,
I'm working on a Projekt, that it should be STM32F7 interfaced with a EDT-Display but without using the Operating System or TouchGFX.
The Developer had designed the Board in a way, that nobody can use it directly without FreeRTOS or TouchGFX.
I've tried to using BSP_Library but not worked. It were designed in order to work only with the internal BootLoader.
The Board which i used shown in Attachement als a Picture and its Model is : ETEMB043013XDHAL
Anybody here have an idea about that?