Question
Error: failed to erase memory
Hello there
I was trying to debug my stm32h750 with an stlink-v3 mini. I'm currently working with an external flash as my code area. The bootloader and external loader worked before, but suddenly I can't load code on my external flash. Does anyone know why this happens?
This is the error I receive when trying to debug:
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 002F00225632500820313236
ST-LINK FW : V3J9M3
Board : STLINK-V3MINI
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev Y
Device name : STM32H7xx
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0xd2
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a30988.srec
File : ST-LINK_GDB_server_a30988.srec
Size : 312284 Bytes
Address : 0x90000000
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 4]
Error: failed to erase memory
Error: failed to erase memory
Shutting down...Thanks