Skip to main content
Graduate
March 25, 2024
Solved

Error in footprint land pattern in STM32G431MB

  • March 25, 2024
  • 1 reply
  • 748 views

@Peter BENSCH 

 

Hi Peter,

Please clarify the foot-print land-pattern in STM32G431MB as shown below. The actual pitch is 0.5 mm and for pins 1 to pin 20, the pitch should be 19*0.5 = 9.5 mm. But it is showing 9.8 mm in the datasheet.

 

sreejithrnair_0-1711347077555.png

Regards,

Sreejith

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @sreejithrnair

    It looks fine on my side since the width of each pin is 0.3 and the distnace between two consecutive pins is 0.2 or we have 20 pins so the total dimension should be : 19*0.2+20*0.3=9.8mm

    Best Regards.

    STTwo-32 

    1 reply

    STTwo-32Answer
    Technical Moderator
    March 25, 2024

    Hello @sreejithrnair

    It looks fine on my side since the width of each pin is 0.3 and the distnace between two consecutive pins is 0.2 or we have 20 pins so the total dimension should be : 19*0.2+20*0.3=9.8mm

    Best Regards.

    STTwo-32