Error in initializing ST-LINK device in the STM32 Nucleo-144 evaluation board
Hi guys
I am using the STM32 Nucleo-144 evaluation board and trying to upload the program by the STM32 ST-LINK Utility.
When I try to connect to the board, the console always shows the following error message: "No target connected," "Can not connect to target!"
At the same time, an Error occurred in initializing the ST-LINK device.
Reason: USB communication error. Please reconnect the ST-LINK USB cable and try again.
I changed the USB cable, but the phenomenon is the same.
And also checked the VDD power on the board, and all of the digital power is in normal operation.
What can I check more to solve the reasons for this issue?