Skip to main content
Visitor II
April 14, 2021
Solved

Error in initializing ST-Link device. Reason: (-1) Unknown. Please check power and cabling to target.

  • April 14, 2021
  • 1 reply
  • 3894 views

When I tried to debug my STM32F303RE nucleo board with Truestudio , I get this messages from console:

When I get this message , I was working on EXTI interrupts at register level

STMicroelectronics ST-LINK GDB server. Version 5.1.0
Copyright (c) 2018, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 LogFile Name : D:\projeler\sf_projeler\Attolic_workspace\EXTI2_example\Debug\st-link_gdbserver_log.txt
 Logging Level : 31
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Enabled
 SWD Debug : Enabled
 
Hardware watchpoint supported by the target 
SWD frequency = 4000 kHz
ST-LINK Firmware version : V2J37S27
Device ID: 0x446
PC: 0xfffffffe
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.

I was able to program it even last night , but this morning suddenly occur this error.

Now , I can program it with stm32cube programmer .

What I did to solve it:

  • upgraded firmware of ST-link .
  • connected with STM32CUBE programmer and full erase chip succesfully.
  • reinstall Truestudio

thanks.

    This topic has been closed for replies.
    Best answer by AAdin.1

    SOLVED!!

    It is solved again suddenly :D :D :D

    I writed this post and ı walked at park about 1-2 hours.

    When I checked again , I surprised .

    Anyone can explain why happend this ?

    -met

    1 reply

    AAdin.1AuthorAnswer
    Visitor II
    April 14, 2021

    SOLVED!!

    It is solved again suddenly :D :D :D

    I writed this post and ı walked at park about 1-2 hours.

    When I checked again , I surprised .

    Anyone can explain why happend this ?

    -met