Skip to main content
Explorer
June 3, 2024
Question

"Error in initializing ST-LINK device. Reason: No device found on target." STM32H743IIT6

  • June 3, 2024
  • 1 reply
  • 600 views

I desinged a custom board using STM32H743IIT6. But I can't Debug it.

  • Reset is pulled high
  • Boot0 is pulled low
  • VDD is stable at 3..28V at all desired pins of the board
  • VCAP 1&2 connected to 2.2uF capacitors...
  • VDDA is 3.28V, VSSA is Grounded

    I tried manything but I couldn't debug it. Using ST-LinkV2.
    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 25, 2024

    Hi @_CEVVAL ,

    Some recommendations:

    -Amel