Question
Error initializing ST-Link device
Posted on June 20, 2012 at 22:59
First post here.
I have been programming the stm32f0 discovery kit for a few days now using the Atollic gdb server with no problems whatsoever, that is until today. I was in the middle of debugging and lost the link to the stm32f0, now when I try to reinitialize the device I get the initialization error. I can use the stm stlink utility and load a hex file with no problems. I actually reloaded the same program I was working on when I lost the link. I have the Stm32f4 discovery board as well and I connected that to see if it was a driver issue but I have no problems initializing the st-link on that board. I connected the f0 board to another computer I have and I cant get it to initialize the st-link either. Does anyone have any suggestions for a fix, Im at a loss here. thanks Tim oh by the way there is a new arm forum called Arm-hq go here: http://forum.arm-hq.com It needs more members so sign up #stm32 #st-link #stm32f0