Skip to main content
Visitor II
September 28, 2022
Question

"Error: Initializing the option bytes failed" when trying to connect with device in dfu mode

  • September 28, 2022
  • 1 reply
  • 2811 views

Hi all,

I'm using STM32F767 Microcontroller.

For flashing FW to the controller I'm using STM32CubeProgrammer through USB DFU mode.

By making the BOOT pin high, I tried to connect the device with programmer through USB.

Then I observed the error screen pop-up shoeing "error: initializing option bytes failed".

This is not happening in all PCBs. It happened only in some PCBs.

Attached the screenshot for your reference.

Can anyone help me in knowing why this error message is coming and how to fix this.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 11, 2022

    Hello @Snulu.1​,

    I was wondering if you are facing the same issue. Could you try to check your boot configuration using AN4661 section 4 Boot configuration. Also verify your boot pin connection in the following section.