Error: No STM32 target found!
Hello,
i am using STM32H735G-DK. everything was good i programmed the board more times and it was working fine. but now I have no idea what happened with my board. i tried to upload firmware using stm32 programmer but problem is as it is.
15:10:51 : STM32CubeProgrammer API v2.12.0 | Windows-64Bits
15:11:33 : ST-LINK SN : 001F00303438510734313939
15:11:33 : ST-LINK FW : V3J10M3
15:11:33 : Board : STM32H735G-DK
15:11:33 : Voltage : 0.12V
15:11:33 : No STM32 target found!
15:11:33 : ST-LINK SN : 001F00303438510734313939
15:11:33 : ST-LINK FW : V3J10M3
15:11:33 : Board : STM32H735G-DK
15:11:33 : Voltage : 0.10V
15:11:33 : Error: No STM32 target found!
Please anybody let me know if you have any suggestion to solve the issue. i have already tried below solution mentioned in STM32H735G-DK manual still problem not resolved.
If a deadlock occurs because of a mismatch between hardware and firmware PWR settings (SMPS/LDO), the user can recover the board by applying the following procedure:
1. Power off the board.
2. Set SW1 (BOOT0) to 1 (system memory). This changes the BOOT0 pin to 1 instead of 0, thus changing the device boot address to boot address 1 and making the bootloader start in System memory. This avoids starting firmware in the user Flash with a wrong SMPS/LDO configuration versus the hardware board configuration.
3. Power on the board and connect using STM32CubeProgrammer (STM32CubeProg). 4. Erase the user Flash.
5. Power off the board and set SW1 to 0.
6. The board is recovered and can be used normally with matching firmware PWR.