Error: No STM32 target found! on custom board
Hi,
I have designed a custom board based on a F417, I am trying to program it with an ST-Link V2 through SWD(SWCLK, SWDIO, GND and RST) and I only get: Error: No STM32 target found!
I have tried the CubeProgrammer, the STLink Utility, the CubeIDE, with modes Normal, Under Reset, Power Dowm... and nothing works.
The PCB traces are connected directly from the SWD header to the pins, but I have also tried with some PullUp-Down resistor on the lines, as a few designs have, and nothing...
I attach a screencapture of the PCB design file, 4 layers, used top and bottom for signals, 2nd for GND and 3rd for 3.3V, 100nF for each VDD pin...
I have tested all the sldering, and it is correct too.
I don't know what can I do from now.
Thank you so much
Best regards