Error: target voltage may be too low for reliable debugging
I have an Nucleo F401RE Board where i broke of the stlink part.
Now i try to use this stlink part to programm and debug an stm32f401cc blackpill board.
I works that i can flash my code onto the blackpill mcu (using platformio and openocd), but i always get the following error message:
Error: target voltage may be too low for reliable debugging.
If i try to start a debug session it won't work.
The STM32CubeProgrammer shows the voltage of the board 0,1V.
I connected a 3,3V pin on the blackpill to the VDD pin on the SWD header at the stlink.
Don't know what i am missing here? Maybe someone can help?