Skip to main content
Visitor II
October 10, 2021
Question

Error when trying to run a program on STM32F7508-DK with OpenOCD

  • October 10, 2021
  • 0 replies
  • 610 views

Hi,

I'm working on a STM32F7508-DK recently bought. I've imported an example project from stm32f7 packages called Menu_Launcher. I'm trying to run the project with OpenOCD but this doesn't work and I have the following errors in the console :

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J38M27 (API v2) VID:PID 0483:374B

Info : Target voltage: 3.228947

Info : clock speed 4000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x5ba02477

Warn : Silicon bug: single stepping may enter pending exception handler!

Info : STM32F750N8Hx.cpu: hardware has 8 breakpoints, 4 watchpoints

Info : STM32F750N8Hx.cpu: external reset detected

Info : starting gdb server for STM32F750N8Hx.cpu on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x08002b48 msp: 0x20050000

Info : device id = 0x10016449

Info : flash size = 64 kbytes

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x08002b48 msp: 0x20050000

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x08002b48 msp: 0x20050000

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x08002b48 msp: 0x20050000

shutdown command invoked

Info : dropped 'gdb' connection

shutdown command invoked

I've tried to use stm32 ST-LINK Utility to see if the board is locked or something like this but I can flash it so I don't think that the problem comes from the board. And the connection speed seems to be good aswell.

Did someone have the same issue and could solve it ? Or do you have ant ideas of where the problem could come from ?

Thanks by advance

    This topic has been closed for replies.