Eval Board ADXL354
Hey everyone,
I am working with the ADXL 354 eval board with an STM32H745
data sheet ADXL354 : https://www.analog.com/media/en/technical-documentation/data-sheets/adxl354_adxl355.pdf
data sheet eval boad: https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADXL354-355-UG-1030.pdf
I have configured the pin PA0-C for the ADC.
I have connected all the pin as indicate in the datasheet (exept the VDDIO and GND of the RANGE and Mode because if i do so, the thing is not working at all) but the output is always the maximum (if my ADC is configured as 8 bit, the accelerometer returns 255)
If I move nothing change. So I connected the GND of MODE and RANGE and I have value (again if I connect the VDDIO of RANGE and MODE, it is not working at all) but my acceleremeter become really really hot (not brun but...)
Can you help me with that ?
Thanks ;)