Skip to main content
Visitor II
December 7, 2023
Solved

Evaluation board for STMF427

  • December 7, 2023
  • 2 replies
  • 1829 views

Hello,

I am looking for a evaluation board for STMF427 MCU. Is the board NUCLEO-F429ZI the right evaluation board for it?

Are the MCUs F427 and F429 different from each mainly from graphic features like the display interface?

 

Kind regards,

Neo

 

    This topic has been closed for replies.
    Best answer by waclawek.jan

    Yes, the 'F427 and 'F429 differ only in absence of LTDC in 'F427 (more precisely, it is the same silicon chip, except in the 'F427 the LTDC is not tested thus not guaranteed to work, may be blocked in some way, and possibly may be removed in the future).

    So, you can use also any 'F429 board as an evaluation board for 'F427.

    JW

    2 replies

    ST Employee
    December 7, 2023

    Hi,

    You can use NUCLEO-F429ZI as evaluation board for STM32F427. The difference is F429 can support LCD-TFT. 

    nanjunAuthor
    Visitor II
    December 7, 2023

    Thank you!

    Super User
    December 7, 2023

    Yes, the 'F427 and 'F429 differ only in absence of LTDC in 'F427 (more precisely, it is the same silicon chip, except in the 'F427 the LTDC is not tested thus not guaranteed to work, may be blocked in some way, and possibly may be removed in the future).

    So, you can use also any 'F429 board as an evaluation board for 'F427.

    JW

    nanjunAuthor
    Visitor II
    December 7, 2023

    Thank you JW for this detailed answer!